Part Number: MSP-EXP432E401Y
Other Parts Discussed in Thread: TPS2052B
Hi,
I am currently using MSP-EXP432E401Y, with default power selection. Means I am using power from debug. Now I want to apply the power externally through 5V supply. Does it also require the 3.3V externally apart from the 5V? If you have any suggestion related to external power design than please share. Another thing is if I keep the power option on debug port not externally than if I want to drive the MOSFET gate in my circuit then is it possible with this power selection? Means, if I isolate the port pin through the opto and connect the MOSFET on the other side of the opto with board 5V then will it work smoothly? In my application I need to run 8 MOSFET so please reply accordingly.
thanks,
Kaushik