This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/MSP432E411Y: Resource Explorer: SimpleLink MSP432E4 SDK - v:2.10.00.17

Part Number: MSP432E411Y

Tool/software: Code Composer Studio

Hi all,

For some reason, on the Resource Explorer under SimpleLink MSP432E4 SDK - v:2.10.00.17/examples/DevelopmentTools/MSP432E401Y LaunchPad, all of the folders are empty when you follow them to the root. For example, when I try to open up  SimpleLink MSP432E4 SDK - v:2.10.00.17/examples/DevelopmentTools/MSP432E401Y LaunchPad/TI-RTOS Kernel/benchloop/Ti-RTOS/CSS_Compiler/benchloop , there is nothing in the folder. And it is the same for the entire Examples folder for this specific SDK. Can someone help me find these Examples? Thanks.

  • Hello Ryan,

    Resource Explorer is cloud based.  You can click on 'benchloop' and import the project to your IDE by clicking the Code Composer icon shown at the top right hand corner.  The project along with the code files should appear in Project Explorer of your IDE.

    Regards,

    Arthi

**Attention** This is a public forum