This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: Code Composer Studio
hi this is harikrishna..
I am doing the project based on LPM modes ..after all the documenteation have read..i going to using the LPM4 mode in my project..
when i checking the examples in the ccs resource explore i am not getting the current consumption in uA ..i am getting the values in mA..i am giving the externer vcc 3.3 volts to the mcu and checking for the mcu load..
for the execution it is taking 230mA and more ..after enters to the LPM4 it is still taking in mA(20,10) current.. not enter to the uA..after removing the debugeer also still in mA(10) only..please give a suggestion
to enter LPM4 properly...
**Attention** This is a public forum