Part Number: MSP430F67791
Other Parts Discussed in Thread: MSP430F6736
Hi every one
I have worked on the single phase meter EVM430-F6736 and I combined the old version of the library dlms cosem with the firmware emeter-6736A.ewp but I have a problem with the call of the function process_rx_frame (& link [1] , & rx [1]); when I compile the IAR the program will execute automatically without clicking on the RUN button and as it progresses it enters an infinite loop. If there is a solution to solve the problem.
Thank you