Part Number: MSP432P401R
Other Parts Discussed in Thread: MSP-FET
Hello,
I am attempting to upload an example program using the BSL scripter on the MSP432P401R Rev 2.0 Launchpad. It gets stuck on the initialization.
Input file script is: C:/.../ScriptExampleWIndows/P4xx_uart/script_P4xx_uart.txt
MODE P4xx UART 9600 COM4 PARITY
[ERROR_MESSAGE]Initialization of P4xx BSL failed! Exit the scripter!
Looking at the source code for the BSL-Scripter, I see this error happens when it fails to receive an ack of 0x00. I have tried:
1. Factory Reset
a. Project Properties > Debug > MSP432 Settings > Erase Method > Erase main and information memory
b. Allow BSL information memory erase
2. Toggle Reset on board
Any help would be appreciated.
Thanks,
Zach