This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I want to use I2C for BSL. How can I design the hardware and is there any example code for MSP430F5234 implementing I2C BSL? Thanks.
Best regards,
Penny
Hi Jace,
The Test +RST pins are always required for BSL, right? I was copying the schematic of Target-Socket MSP-TS430RGC64C, but RST pin was missing from the BSL Interface pins. We need to add RST pin to pin 4 in order to use BSL rocket to run scripter, is that correct?
As BSL rocket and BSL scripter support both I2C and UART, how can I design the hardware to support I2C BSL?
Can I connect SDA and SCL to the BSL connector? And besides the I2C pins, TEST, RST, DVCC and DVSS should be the same, right?
Another question about the target socket board: why do you have two 26Mhz crystal on the board while MSP430 device only support 25Mhz system clock? Thanks.
Best regards,
Penny
**Attention** This is a public forum