This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430G2553: ADC Problem and ADC internal resistance?

Part Number: MSP430G2553

Hello Guys,

I want to measure the high voltage so i use Voltage dividing circuit and

read adc value but some problem is appear;

then in programe  i use vcc for reference;

adc=ADC10MEM;

voltage 1 = adc*3.3/1023;                 (ADC measure Voltage)

voltage 2 = voltage 1 * (R2+R1)/R1 (VCC VOLTAGE)

it strange then value is not correctly to three-meter;

for emaple 30V -VCC then the result like picture;

note:adc value measure is Equivalent to three-meter

**Attention** This is a public forum