Part Number: MSP430G2553
Hello everyone, I’m currently having an issue getting the SEN0160 weight sensor to work with the MSP430g2553. The SEN0160 uses the HX711 ADC chip (all datasheets attached below). I am not able to read the data coming from the chip and it’s definitely a hardware issue because I measured the voltage at the load cell connections and I’m getting a measured voltage of 2.5 at the E+ port. According to the datasheet the range is 2.6-5.5 V. The load cell itself I think needs 5 volts excitation, but I’m not even reaching the minimum 2.6 volts when I’m powering the hx711 ADC with 5 volts through a 5 Volts DC power supply. I posted some pictures below to help clarify. I actually connected the DOUT and SCK pins to P2.3 and P2.4 not the uart pins as shown below.
https://www.dfrobot.com/wiki/index.php/Weight_Sensor_Module_SKU:SEN0160