This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: Code Composer Studio
Dear all,
It might come off as a stupid question, but I would really appreciate if you could help me out, it is pertaining to the ADC interrupt. So, the MSP430i2041 has SD24 ADCs, which does 'single channel single conversion', 'single channel continuous conversion', and the same with multiple channels. Now using interrupts, the CPU is left unengaged and free to perform other operation while the data acquisition is being performed by ADC? If yes, then how many clock cycles (or how much time) do I have to perform CPU operation on previously acquired ADC data before the new one arrives (at fm = 1MHz, and Oversampling ratio of 256)?
If there's a text explaining all of this and some more, I would really appreciate being pointed towards it.
Thank you.
P.s., I have a real hard time understanding the concept of interrupts, would appreciate some help in this regard too.
With Warm Regards
Neal
**Attention** This is a public forum