This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/MSP430FR5994: FRAM read/write power consumption using EnergyTrace

Part Number: MSP430FR5994
Other Parts Discussed in Thread: ENERGYTRACE,

Tool/software: Code Composer Studio

Hi,

I'm trying to determine how much power is consumed when copying two data buffers (~3KB in total)  to/from SRAM <-> FRAM. I'm using memcpy to copy data between SRAM and FRAM, not using DMA.

I'm trying to use EnergyTrace (CCSv8) for this purpose. I have set markers in the code (e.g. toggling GPIO / output to UART etc.) but these markers are not seen in the Energy Trace power output (attached).

The initial spike seen is I think the clocks being setup ?, but where's the gpio toggling power consumption ?

The whole FRAM<->SRAM data transfer takes about 3ms each, so i've zoomed in the plot.

CPU is running in Active power mode. Energy trace is used in standalone mode.

Is there a better way to determine the power consumption for a FRAM read/write ?

Thank you

I have some code like the following:

/*
 * main.c
 *
 */

#include "conf.h"
#include "utils/myuart.h"


/*******************************************************
 * Globals
 *******************************************************/
unsigned char Buff_First[16*96];
unsigned char Buff_Second[16*96];

uint8_t *Buff_First_ptr = (uint8_t *)&Buff_First;
uint8_t *Buff_Second_ptr = (uint8_t *)&Buff_Second;



/*******************************************************
 * FUNC DEFS
 *******************************************************/

void benchmark_buff_checkpoint_latency(void);

/*************************************************************************************
 * MAIN
 *************************************************************************************/
void main(void)
{
    /* mandatory init stuff */
    WDTCTL = WDTPW | WDTHOLD;     //Stop WDT
    PM5CTL0 &= ~LOCKLPM5; // Disable the GPIO power-on default high-impedance mode to activate previously configured port settings

    system_init(); // init clocks, UART
    setupDebugPins(); // setup pins as output GPIO pins

    benchmark_buff_checkpoint_latency();

    while(1){
	__no_operation();
	}
}


/*************************************************************************************
 * BENCHMARKING
 *************************************************************************************/
void benchmark_buff_checkpoint_latency(void){

    _DBGUART("aaaaaaaaaaaaaaaaaaaaaaaaaaaaaaaaaaaaaaaaaa %d \r\n", 123);
    _DBGUART("aaaaaaaaaaaaaaaaaaaaaaaaaaaaaaaaaaaaaaaaaa %d \r\n", 123);
    GPIO_toggleOutputOnPin( GPIO_PORT_P1, GPIO_PIN1 );
    GPIO_toggleOutputOnPin( GPIO_PORT_P1, GPIO_PIN1 );
    GPIO_toggleOutputOnPin( GPIO_PORT_P1, GPIO_PIN1 );

    /* from SRAM to FRAM */
    Buffer_backup(Buff_First_ptr, Buff_Second_ptr);

    _DBGUART("aaaaaaaaaaaaaaaaaaaaaaaaaaaaaaaaaaaaaaaaaa %d \r\n", 123);
    _DBGUART("aaaaaaaaaaaaaaaaaaaaaaaaaaaaaaaaaaaaaaaaaa %d \r\n", 123);
    GPIO_toggleOutputOnPin( GPIO_PORT_P1, GPIO_PIN1 );
    GPIO_toggleOutputOnPin( GPIO_PORT_P1, GPIO_PIN1 );
    GPIO_toggleOutputOnPin( GPIO_PORT_P1, GPIO_PIN1 );

    /* from FRAM to SRAM */
    Buffer_restore(Buff_First_ptr, Buff_Second_ptr);

    _DBGUART("aaaaaaaaaaaaaaaaaaaaaaaaaaaaaaaaaaaaaaaaaa %d \r\n", 123);
    _DBGUART("aaaaaaaaaaaaaaaaaaaaaaaaaaaaaaaaaaaaaaaaaa %d \r\n", 123);
    GPIO_toggleOutputOnPin( GPIO_PORT_P1, GPIO_PIN1 );
    GPIO_toggleOutputOnPin( GPIO_PORT_P1, GPIO_PIN1 );
    GPIO_toggleOutputOnPin( GPIO_PORT_P1, GPIO_PIN1 );

}


  • I guess the issue might be related with granularity ?

    I proceeded with the following:

    I ran the memcpy (SRAM <-> FRAM) iteratively for 1000 times as below:

    for (i=0;i<1000;i++){
            Buff_backup(Buff_First_ptr, Buff_Second_ptr); // copy both buff1 and buff2 to FRAM from SRAM using memcpy
        }
    

    same as above for reading back from FRAM to SRAM.

    And I got the below.

    According to this, FRAM write consumes much more power than FRAM reads.

    FRAM write = ~1mW,

    FRAM read = ~0.2mW

    Am I reading this measurement correctly ?

    Is there a way to find out the energy consumed during only the read/write periods ?

    thanks

  • Hi Rosh,

    First I'm trying understand how you are accessing FRAM?
    Unless I missing something here, the two buffers you have declared in your example are placed in RAM by the compiler.
  • Hi Dennis,

    Correct - the two buffers are in SRAM, then inside Buff_backup(Buff_First_ptr, Buff_Second_ptr);, memcpy is used to copy both first and second buffer to two buffers in FRAM. like so:

    void Buff_backup(uint8_t *buff1_ptr, uint8_t *buff2_ptr){
    
    memcpy(Buff_First_FRAMStorage_ptr, buff1_ptr,   16*96);
    memcpy(Buff_Second_FRAMStorage_ptr, buff2_ptr,   16*96);
    
    }

    eg. of how the buffer is in FRAM (compiler/linker decides on the fram location):

    #pragma PERSISTENT(Buff_First_FRAMStorage)
    unsigned char Buff_First_FRAMStorage[16*96] = {0};

    and then i do the reverse memcpy, to copy from FRAM back to SRAM.

    it's worth mentioning i'm using clock SMCLK=MCLK=8MHz.

    so two questions:

    1) why is my FRAM read energy/power different to the FRAM write ?

    2) at 8MHz, does SRAM and FRAM have the same r/w latency & energy ? if yes, why do we need to use SRAM at lower clock speeds ?

    thanks

  • Hi Rosh,

    Ok.  Let's try this...in CCS on the menu on the top you can select View>Expressions to open an expressions window.

    In the expression window, add your variable names and tell me what address they are located at.

    I did something similar.  See below.  Notice that my variable 'buffer' is assigned to RAM.  My other variable 'FRAM_buffer' is assigned to FRAM, but I had to use the #pragma PERSISTENT in order for the linker to place it there.

    Also, take a look at the MSP430 FRAM Technology - How To and Best Practices.

  • Hi Dennis,

    that is what I did as well. see code and screenshot attached, to confirm what you have said.

    main_pdi_exp_rawbenchmarking.c
    Fullscreen
    1
    2
    3
    4
    5
    6
    /*
    * main.c
    *
    * Created on: Nov 27, 2018
    * Author: Rosh
    *
    XXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXX

    code:

    #define BUFF_SIZE 16*96
    
    // buffers in SRAM
    unsigned char SRAM_Buff1[BUFF_SIZE];
    unsigned char SRAM_Buff2[BUFF_SIZE];
    
    // buffers in FRAM
    #pragma PERSISTENT(FRAM_Buff1)
    unsigned char FRAM_Buff1[BUFF_SIZE] = {0};
    #pragma PERSISTENT(FRAM_Buff2)
    unsigned char FRAM_Buff2[BUFF_SIZE] = {0};
    

    memory locations:

    .bss       0    00001c00    00000c94     UNINITIALIZED
                      00001c00    00000600     (.common:SRAM_Buff1)
                      00002200    00000600     (.common:SRAM_Buff2)

                     
    .TI.persistent
    *          0    00004000    00000c02     
                      00004000    00000600     main_pdi_exp_rawbenchmarking.obj (.TI.persistent:FRAM_Buff1)
                      00004600    00000600     main_pdi_exp_rawbenchmarking.obj (.TI.persistent:FRAM_Buff2)

    confirmed the above locations in watch expressions as well. locations are as above.

    Strange though, on the *.map file the length = 600 for the buffers, but in the CCS memory allocation window and the watch expressions windows show that the length = 1536 (BUFF_SIZE). why is *.map reporting differently ?

    anyway, sticking to the topic, when I run the attached code, i get this :

    FRAM Read energy is lower than FRAM Write, but speeds are the same.

    same buffer size. using 1000 runs of memcpy.

    Why is this ?

  • When I remove memcpy and simply copy data in a loop :

    /* fram write */
        for(i=0; i<1000; i++){
            for (j=0;j<BUFF_SIZE;j++){
                FRAM_Buff1[j]=SRAM_Buff1[j];
            }
            for (j=0;j<BUFF_SIZE;j++){
                FRAM_Buff2[j]=SRAM_Buff2[j];
            }
        }
    
        _delay(1000000);
    
        /* fram read */
        for(i=0; i<1000; i++){
            for (j=0;j<BUFF_SIZE;j++){
                SRAM_Buff1[j]=FRAM_Buff1[j];
            }
            for (j=0;j<BUFF_SIZE;j++){
                SRAM_Buff2[j]=FRAM_Buff2[j];
            }
        }
    

    I get the opposite behavior (reads consume more power than writes).. very strange..

    of course, in the above (and also in the memcpy case), every FRAM read incurs a SRAM write and vice versa. but it still doesn't explain the asymmetric power consumption behavior.

    Any thoughts ?

  • Hi Rosh,

    My apologies to you for noticing your FRAM memory allocation earlier.
    I looked at the disassembly of your code and didn't see anything strange there.
    My understanding is the power should be fairly equal in both scenarios, so let me contact our FRAM memory expert.

    To answer your question regarding the reported buffer length, 600hex = 1526dec.

    BTW, what compiler optimization setting to you use?
  • Hi Dennis,

    I looked at my disassembly, and something strange came up.

    171         for(i=0; i<1000; i++){
    01041c:   430E                CLR.W   R14
    01041e:   903E 03E8           CMP.W   #0x03e8,R14
    010422:   2C1A                JHS     (0x0458)
    172             for (j=0;j<BUFF_SIZE;j++){
            $C$L13:
    010424:   430F                CLR.W   R15
    010426:   903F 0600           CMP.W   #0x0600,R15
    01042a:   2C07                JHS     (0x043a)
    173                 SRAM_Buff1[j]=FRAM_Buff1[j];
            $C$L14:
    01042c:   4FDF 4000 1C00      MOV.B   0x4000(R15),0x1c00(R15)
    172             for (j=0;j<BUFF_SIZE;j++){
    010432:   531F                INC.W   R15
    010434:   903F 0600           CMP.W   #0x0600,R15
    010438:   2BF9                JLO     (0x042c)
    175             for (j=0;j<BUFF_SIZE;j++){
            $C$L15:
    01043a:   430F                CLR.W   R15
    01043c:   903F 0600           CMP.W   #0x0600,R15
    010440:   2C07                JHS     (TA3_TA3R)
    176                 SRAM_Buff2[j]=FRAM_Buff2[j];
            $C$L16:
    010442:   4FDF 4600 2200      MOV.B   0x4600(R15),0x2200(R15)
    175             for (j=0;j<BUFF_SIZE;j++){
    010448:   531F                INC.W   R15
    01044a:   903F 0600           CMP.W   #0x0600,R15
    01044e:   2BF9                JLO     (TA3_TA3CCTL0)
    171         for(i=0; i<1000; i++){
            $C$L17:
    010450:   531E                INC.W   R14
    010452:   903E 03E8           CMP.W   #0x03e8,R14
    010456:   2BE6                JLO     (0x0424)
    

    above section is for the below C code:

    /* fram read */
        for(i=0; i<100; i++){
            for (j=0;j<BUFF_SIZE;j++){
                SRAM_Buff1[j]=FRAM_Buff1[j];
            }
            for (j=0;j<BUFF_SIZE;j++){
                SRAM_Buff2[j]=FRAM_Buff2[j];
            }
        }

    What I'm confused is why are there references to Timers in the loop ?? (highlighted above in bold : e.g. TA3_TA3R, TA3_TA3CCTL0


    it should be a straightforward, compare and jump if hi/low right ?

    could this be the reason my FRAM read is acting strange ?

    there is some other code in the project that is being built, but they are not being included or executed. (no *.h being included from the other project files), so it cant be external interference could it ?

    below are my compiler settings :

    -vmspx --data_model=restricted --use_hw_mpy=F5 --include_path="${CCS_BASE_ROOT}/msp430/include" --include_path="${workspace_loc:/${ProjName}/driverlib/MSP430FR5xx_6xx}" --include_path="${workspace_loc:/${ProjName}/EPD_drivers}" --include_path="${workspace_loc:/${ProjName}/EPD_drivers/FPL_drivers}" --include_path="${workspace_loc:/${ProjName}/EPD_drivers/Images}" --include_path="${workspace_loc:/${ProjName}/Experimental}" --include_path="${workspace_loc:/${ProjName}/gfxlib}" --include_path="${workspace_loc:/${ProjName}/HW_drivers}" --include_path="${workspace_loc:/${ProjName}/utils}" --include_path="${PROJECT_ROOT}" --include_path="${CG_TOOL_ROOT}/include" --advice:power=all --advice:hw_config=all --define=__MSP430FR5994__ --define=DEPRECATED --define=USE_EPD_Type=dr_eTC_BWb --define=USE_EPD_Size=sz_eTC_144 --define=eTC_G2_Aurora_Mb_Ext --define=_MPU_ENABLE -g --printf_support=minimal --diag_warning=225 --diag_wrap=off --display_error_number --abi=eabi --silicon_errata=CPU21 --silicon_errata=CPU22 --silicon_errata=CPU40 --small_enum

    --opt_level=0, --opt_for_speed=1, --use_hw_mpy=F5,

    what other options do you need to see ?

  • Hi Rosh,

    I'm still waiting to hear back from our FRAM expert.

    Regarding the references to the TA3 registers, I'm actually not sure, but it looks like the compiler is interpreting these as lower 64K relative addresses and happen to be the same address as some of the TA3 registers.  The correct code is being generated, just a confusing disassembly.

    Here is table from the datasheet:

**Attention** This is a public forum