Part Number: MSP430G2553
Hi,
I just bought the MSP430G2553 microcontroller for a class project and I can't get to try the blink example since it doesn't detect it connected even though I sellected the right micro and it recognizes there are ports and I can select one of them (CAM4 and CAM5, not sure which is which but it doesn't work with any of them). Also, I checked in windows Device Manager those are the ports linked to the microcontroller and installed the Energia drivers for windows 64 bits.
Hope someone can help me out here.
I attach some screenshots down bellow.