This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I just bought the MSP430G2553 microcontroller for a class project and I can't get to try the blink example since it doesn't detect it connected even though I sellected the right micro and it recognizes there are ports and I can select one of them (CAM4 and CAM5, not sure which is which but it doesn't work with any of them). Also, I checked in windows Device Manager those are the ports linked to the microcontroller and installed the Energia drivers for windows 64 bits.
Hope someone can help me out here.
I attach some screenshots down bellow.
I happen to have the G2ET launchpad, so I did as you told me and problem solved.
Thank you very much Bruce!
**Attention** This is a public forum