This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Folks,
For a digital picture frame i would like to use the MSP430 to connect a 20" TFT LCD display (Resolution 1600 X 1200) via SPI. Do you think this is doable? Is there a LCD controller that can support such a high resolution with SPI? In my research so far i have found some projects for small displays such as this:
2.8" display: MSP430FG439: MSP430FG439 LCD Display - MSP low-power microcontroller forum - MSP low-power microcontrollers...
Best Regards.
Ilona
**Attention** This is a public forum