This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/MSP432P401R: I can not use the driver library APIs

Part Number: MSP432P401R

Tool/software: Code Composer Studio

I'm a beginner using the MSP432P401R and I found that I can write code using the driver library but I can not include it in my project. I downloaded an example using the adc14 because I have to use the adc14 for a project, and when I build the downloaded example it works, but as soon as I try making a new project and include the "driverlib.h" it gives me this dialogue: "cannot open source file driverlib.h"

I already tried linking paths in the include options within the properties of the project.

**Attention** This is a public forum