Part Number: MSP432E411Y
I am trying to gather information on programming the MSP432E411Y prior to soldering the device to the PCB.
1. Is it possible to program msp432e411y internal flash( 1MB ) offline ? ( i.e., is there a way to program the internal flash ( 1MB ) first and then solder it into the Card , instead of updating the internal flash after soldering on the Card using Jtag programmer,…?
2. Is it possible to program msp432e411y internal EEPROM ( 6Kbytes ) offline?
3. Is it possible to program msp432e411y internal EEPROM ( 6Kbytes ) using Dediprog or any other Hardware tools ?
Thanks,
Robb