This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP432E411Y: Stand alone programming options for MSP432E411Y

Part Number: MSP432E411Y

I am trying to gather information on programming the MSP432E411Y prior to soldering the device to the PCB.

1. Is it possible to program msp432e411y internal flash( 1MB ) offline ? ( i.e., is there a way to program the internal flash ( 1MB ) first and then solder it into the Card , instead of updating the internal flash after soldering on the Card using Jtag programmer,…?

2. Is it possible to program msp432e411y internal EEPROM ( 6Kbytes ) offline?

3. Is it possible to program msp432e411y internal EEPROM ( 6Kbytes ) using Dediprog or any other Hardware tools ?

Thanks,

Robb

**Attention** This is a public forum