This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I use MSP430F149 for years with same firmware and everything was OK till now. MCUs from last delivery works, but their A/D convertor show results which are lower than real value of measured voltage is. The difference is same for all new MCUs and it's 150mV lower that real voltage is. As a reference is used the internal voltage reference.
Does anybody idea where the problem could be? Is there any change in structure of MCU MSP430F149? Firmware, PCB, everything is same, only A/D measure lower voltage realyty is.
Many thanks in advance for your help / ideas
Kind Regards,
Jiri
Hello JD,
when I use any MCU from new revision (marking on body of IC is: 4CAPC1WG4, M430F149, REV S) all ones give same wrong result of A/D conversion. When I place on the same board MCU from "Old" revision (full marking on the body is: 7AE18ETG4, M430F149, REV N), results from A/D conversions are correct. Of course in ALL MCUs is running same firmware.
Any Idea what is different between both revisions?
Many thanks in advance for your ideas
Best Regards,
Jiri
Hi JD,
I use internal reference voltage 2.5V.
Your notice regarding internal calibration brings solution - my small fault in the routine :-( I several check it, but didn't see. After your notice I said - "There MUST be a mistake" - and I really found it.
Many thanks for your support
Best Regards,
Jiri
**Attention** This is a public forum