This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Was looking at another mpu and wondered, can I put a LP on a breadboard.
Using two Radio Shack BB (the new small ones) connected sideby side.
Using the small part of the header supplied with the LP into the BB.
Going across two BB the LP will fit however tight. I have not soldered yet but it works.
Hi Martin,
so, go ahead and show us your latest developments! Have fun with your Launchpad!
Rgds
aBUGSworstnightmare
Have written a morse code program to mimmic a amature radio message in blinking led.
Proves it is easier to hear than to see. The setup is to a scope to prove code is correct.
So far only have memory for a 32 craracter message.
**Attention** This is a public forum