This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP432P401R: Unable to connect to target after incorrectly setting DCO

Part Number: MSP432P401R

In my 3am stupor I miscounted the number of zeros, and set the DCO to 64MHz using CS_setDCOFrequency(64000000);

Now when I try to program the device (using an MSP FET) I get `CORTEX_M4_0: Error connecting to the target: Unknown device` I am unable to connect to the device to do a factory reset either (CCS V9).

Is there anything I can do to save the MSP or do I just need to abandon ship and resolder a new one on?

**Attention** This is a public forum