Part Number: MSP430F2370
Other Parts Discussed in Thread: TRF7970A, MSP-FET, MSP430FR5969
Hi,
I have a custom board based on MSP430F2370 and TRF7970. The design is based on TI's Ultra-Low Power Card Presence Detection & NFC/RFID Reader reference. Below is the diagram of my 6x2 JTAG on the board and want to know how can I program it ?
Also when I build the example code of NFC reader for MSP430F2370 & TRF7970 I'm getting the below error.(I'm using the CCS 9.0.1)
"This project was created using a version of compiler that is not currently installed - 4.1.2 [MSP430]. See 'Help > Install New Software' and select 'Code Generation Tools Updates' to check if this compiler is available through a CCS update. Visit <a href="liveaction:OpenAppCenter">CCS App Center</a> to get the latest compiler support. Or <a href="software-dl.ti.com/.../a> and install the compiler, then register it with CCS through 'Preferences > CCS > Build > Compilers'. TRF7970A_Ultra_Low_Power_Card_Detection properties Problem"
Regards,
Madhusudhan