Part Number: MSP-TS430RHB32A
Other Parts Discussed in Thread: MSP430I2040
Hi Team,
Please help me answer the follow question from my customer, thank you so much.
Could you tell us about the maximum operating temperature (temperature) of MSP-TS430RHB32A? I checked the document but could not find the description. At present, temperature testing of MSP-TS430RHB32A is being conducted, but the phenomenon of stopping when operating at 80°C for 2 to 3 hours has occurred multiple times. There are only cable and the substrate in the constant temperature bath. The chip itself seems to be possible up to 105°C, MSP-TS430RHB32A I want to know what it is. In addition, the program at the time of evaluation performs AD conversion every 16 ms and outputs it by UART.
Best Regards,
Tom.Liu