This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430F5529: MSP430F5529 communication with another MSP430F5529

Part Number: MSP430F5529

Hello,

I'm designing a new board based on the MSP430F5529. 

The purpose of the board is to sample analog data and send it to another MSP430F5529 on another board about 2 meter away (connected via cable).

I need the communication will be fast ~1Mbps.

I have 2 questions:

1. Can the MSP UART handle that speed over that distance?

2. Can I use the MSP430F5529 USB interface for communication between them? (If yes then how?)

Thanks,

Ofer.

**Attention** This is a public forum