This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: Code Composer Studio
Hi,
I want to use low power mode of MSP430 and I would like to wake it up after 20 mins and read and send the data. What's the best way to achieve this ?
I'm experimenting with LPM3. How can I achieve this using any LPM mode ?
Hi Preetham,
You need to use a timer with a global counter to achieve this, as in G2553 there isn't any timer itself can support up to 20mins single interval.
All you need to do is to initialize the global counter value in the main loop, tick it in the timer's ISR until the value you want, and then use "__bic_SR_register_on_exit(LPM3)" to exit LPM after the ISR.
Below shows a simple pseudo code for your reference. For the timer, you can use either TimerA or WDT+ in G2553, with ACLK as clock source.
in main loop: { ... counter = 0; start_timer(); __bis_SR_register(LPM3 | GIE); ... } in timer ISR: { clear_timer_IFG(); counte++; if(counter == SOME_THRESHOLD) { __bic_SR_register_on_exit(LPM3); } }
Regards,
Harry
Hi Harry,
Thank you so much.
1) With global timer can I achieve this ?
2) Do you have any sample or blog or anything to help me understand further on this ? Thank you for your time on this.
Hi Preetham,
Yes, all timers in G2553 can achieve this.
You can refer to the lpm3 code examples in MSP430Ware.
I attached the code here for your reference.
You need to pay attention that in this code MCU wakes up every 4 second. You can adjust the timer interval and also put a global variables to count the wakeup times to achieve ~20 min.
/* --COPYRIGHT--,BSD_EX * Copyright (c) 2012, Texas Instruments Incorporated * All rights reserved. * * Redistribution and use in source and binary forms, with or without * modification, are permitted provided that the following conditions * are met: * * * Redistributions of source code must retain the above copyright * notice, this list of conditions and the following disclaimer. * * * Redistributions in binary form must reproduce the above copyright * notice, this list of conditions and the following disclaimer in the * documentation and/or other materials provided with the distribution. * * * Neither the name of Texas Instruments Incorporated nor the names of * its contributors may be used to endorse or promote products derived * from this software without specific prior written permission. * * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS" * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE. * ******************************************************************************* * * MSP430 CODE EXAMPLE DISCLAIMER * * MSP430 code examples are self-contained low-level programs that typically * demonstrate a single peripheral function or device feature in a highly * concise manner. For this the code may rely on the device's power-on default * register values and settings such as the clock configuration and care must * be taken when combining code from several examples to avoid potential side * effects. Also see www.ti.com/grace for a GUI- and www.ti.com/msp430ware * for an API functional library-approach to peripheral configuration. * * --/COPYRIGHT--*/ //****************************************************************************** // MSP430G2xx3 Demo - Basic Clock, LPM3 Using WDT ISR, 32kHz ACLK // // Description: This program operates MSP430 normally in LPM3, pulsing P1.0 // at 4 second intervals. WDT ISR used to wake-up system. All I/O configured // as low outputs to eliminate floating inputs. Current consumption does // increase when LED is powered on P1.0. Demo for measuring LPM3 current. // ACLK = LFXT1/4 = 32768/4, MCLK = SMCLK = default DCO ~ 800kHz // //* External watch crystal installed on XIN XOUT is required for ACLK *// // // // MSP430G2xx3 // --------------- // /|\| XIN|- // | | | 32kHz // --|RST XOUT|- // | | // | P1.0|-->LED // // D. Dang // Texas Instruments Inc. // December 2010 // Built with CCS Version 4.2.0 and IAR Embedded Workbench Version: 5.10 //****************************************************************************** #include <msp430.h> int main(void) { BCSCTL1 |= DIVA_2; // ACLK/4 WDTCTL = WDT_ADLY_1000; // WDT 1s/4 interval timer IE1 |= WDTIE; // Enable WDT interrupt P1DIR = 0xFF; // All P1.x outputs P1OUT = 0; // All P1.x reset P2DIR = 0xFF; // All P2.x outputs P2OUT = 0; // All P2.x reset while(1) { int i; P1OUT |= 0x01; // Set P1.0 LED on for (i = 5000; i>0; i--); // Delay P1OUT &= ~0x01; // Reset P1.0 LED off __bis_SR_register(LPM3_bits + GIE); // Enter LPM3 } } #if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__) #pragma vector=WDT_VECTOR __interrupt void watchdog_timer (void) #elif defined(__GNUC__) void __attribute__ ((interrupt(WDT_VECTOR))) watchdog_timer (void) #else #error Compiler not supported! #endif { __bic_SR_register_on_exit(LPM3_bits); // Clear LPM3 bits from 0(SR) }
**Attention** This is a public forum