Part Number: MSP430FR2355
Other Parts Discussed in Thread: MSP430FR5994,
Hi,
I'm new to the MSP430 world...I'm working on a small energy harvesting project
- I'd like to implement a simple / compact DC-DC converter using an MSP430FR23xx. I'd use the timer block to output a PWM signal, the OpAmps to measure the output voltage and form a PI controller. The output voltage of the PI controller I'd feed into the AD-Converter, which then updates the PWN duty cycle. Reading from the ADC and writing to the PWM is certainly possible while the device is awake, but is there a way to achieve this while the device is asleep (LPM3)? The implementation should be as low power as possible.
- Is there or will there soon be a MSP430FR23xx variant (must have OpAmps / Comparators) with DMA included (like the MSP430FR5994)?
Thanks in advance
Eric