This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Device: MSP430F149
I have CCSv4.2 installed and I am using the MSP430-FETUIF jtag interface - all working well together. However, I am looking for a way to program our devices at several different PC stations. All I have seen so far involves the Gang 430 programmer, or using the CCSv4 and MSP430-FET together. Any help? Thanks,
-dma
Also, there is a free version of the elprotronic FlashPro430 programming software at www.elprotronic.com (the full version supports even batch-file controlled programming)
When I started with the 54xx and the MSP-430FETU430IF, I even figured out how to program MSPs using the msp430-jtag toolchain of the mspgcc compiler. Unfortunately, this toolchain didn't support the newer 54xx processors (new JTAG protocol) and for the older 1611/1232 we still use I already had the original parallel programmer. But I got it working.
You still need to (temporarily) install IAR or CCS, to get holfd of the msp430.dll ( and oen or two more) which do the main work (needed for the elprotronic too)
David Albert said:However, I am looking for a way to program our devices at several different PC stations.
i'm partial to the MSP430 Flasher. it's a simple, open source, command line programming tool which doesn't require installation and works with the FET or eZ430 tools.
give it a try.
http://processors.wiki.ti.com/index.php/MSP430_Flasher_-_Command_Line_Programmer
Olimex also has a free flash tool as well as the DLL drivers for their JTAG hardware. It might work with TI's JTAG tools as well.
Hi Ed,
ever clicked the wiki link http://processors.wiki.ti.com/index.php/MSP430_Flasher_-_Command_Line_Programmer posted by Adrian?
Everything you need to know for using the tool is there!
Rgds
aBUGSworstnightmare
Hello...yes...thats where I got the download...
I am confident I have everything set up properly, but keep getting the following:
Initializing interface on TIUSB Port...
# ERROR 1014: Could not initialize device interface
My batch file specifcially specifies the LPTn option, but it looks as if it is still trying to access using the MSP-FETU430IF versus the LPT Emulation tool.
I am going to try and install the USB drivers and locate a USB Emulator...but I would prefer to use the LPT...any thoughts?
Ed Wilkolaski said:My batch file specifcially specifies the LPTn option
hi ed - are you specifying the LPT com port you're using? it's not obvious, but the n in LPTn is supported to be replaced by the COM port. on my PC, i use "LPT1".
Hello Adrian...
I think we are all set now....I had to uninstall the USB Drivers...then re-install. For whatever reason...that opened up com for both the USB and LPT...thx!
Taht being said...I think I have one more question...
I store my checksum at "0xF800"...I was hoping the '-r' command would allow me to dump the checksum into a text file for viewing. However it looks as if I can only access the MAIN, INFO, RAM, BSL. Is there a way I can dump a specified range of memory into the text file?
Thx
**Attention** This is a public forum