This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/MSP430FR5994: How to write pre-trained model data into FRAM

Part Number: MSP430FR5994


Tool/software: Code Composer Studio

Hi,

I am doing light-weight Machine Learning with the MSP430FR5994 launchpad. I trained the model off-line and I need to upload the trained model data to the launchpad. I am using CCS to program the board. The trained model data should be saved in a float_point array which resides in FRAM. I used PERSISTENT to declare the variable. 

#pragma LOCATION(model, 0x14800);
#pragma PERSISTENT(model);
float model[width][length] = {0};    

How can I write pre-trained model data into this variable while I am programming the board with CCS?

Thanks,

Yubo

  • Hi Yubo,

    If the data won't be modified, then using const to declare the variable is more suitable.  There are two suggestions to upload the model data.

    1. Declare the float model[width][length] variable in a C file with it's initial value as below. These can be performed by a little PC program which reads the model data file in PC and generates the C file automatically. 

    float model[width][length] = { 0.1, 0.2, 0.3, ...};

    2. Using BSL to upload the model data to it's memory space. This can update the model date without re-programming the code. Please see MSP430 BSL page for more information. 

      Bootloader (BSL) for MSP low-power microcontrollers

  • Hi Winter,

    Sorry, I did not explain well. My system does on-device training too, which means the float model array needs to update on the fly and I can not use const. Anyway, I will try your suggestions. 

    Thanks,

    Yubo

  • OK. I'll close this thread. You can still reply this post if any questions or create a new post.

**Attention** This is a public forum