This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: Code Composer Studio
I'm not sure if this is a bug with the MSP430 header or with TCAN4550, but I'd say that using a preprocessor definition for something as commonplace as "ID", is bad practice. See line 4968 of the official msp430fr2355.h - other devices might be affected too.
This causes code like
typedef struct {
uint32_t ID : 29; //...
to fail, as ID for the compiler is now a 0x00c0 constant...
Hi,
I'm not clear about your issue or question. Could you share me details about your issue? Maybe an example code and some compiling error message should be helpful.
Wei,
this is the compiler error:
>> Compilation failure
subdir_rules.mk:7: recipe for target 'uart.obj' failed
Building file: "../tcan4x5x/TCAN4550.c"
Invoking: MSP430 Compiler
"/home/zoe/ti/ccs920/ccs/tools/compiler/ti-cgt-msp430_19.6.0.STS/bin/cl430" -vmspx --data_model=large -Ooff --opt_for_speed=5 --use_hw_mpy=F5 --include_path="/home/zoe/ti/ccs920/ccs/ccs_base/msp430/include" --include_path="/home/zoe/ti/ccs920/ccs/ccs_base/msp430/include" --include_path="/home/zoe/projects/akupakk/software/firmware" --include_path="/home/zoe/ti/ccs920/ccs/tools/compiler/ti-cgt-msp430_19.6.0.STS/include" --include_path="/home/zoe/projects/akupakk/software/firmware/driverlib/MSP430FR2xx_4xx" --advice:power="all" --advice:hw_config="all" --define=DEBUG_ON --define=__MSP430FR2355__ -g --c11 --printf_support=minimal --diag_warning=225 --diag_wrap=off --display_error_number --silicon_errata=CPU21 --silicon_errata=CPU22 --silicon_errata=CPU40 --preproc_with_compile --preproc_dependency="tcan4x5x/TCAN4550.d_raw" --obj_directory="tcan4x5x" "../tcan4x5x/TCAN4550.c"
(...)
gmake: *** [uart.obj] Error 1
"../tcan4x5x/TCAN4x5x_Data_Structs.h", line 524: error #41: expected an identifier
"../tcan4x5x/TCAN4x5x_Data_Structs.h", line 565: error #41: expected an identifier
"../tcan4x5x/TCAN4550.c", line 897: error #135: expected a field name
"../tcan4x5x/TCAN4550.c", line 899: error #135: expected a field name
The code in question is: (line 521 of the official TCAN4x5x_Data_Structs.h)
typedef struct
{
//! @brief CAN ID received
uint32_t ID : 29;
//! @brief Remote Transmission Request flag
uint8_t RTR : 1;
The problem originates from the official msp430fr2355.h; if a file includes both the TCAN data structs header, and the msp430fr2355 header, the preprocessor replaces the word ID with the constant 0x00c0, which causes an error: the compiler wants an identifier in the struct, but sees a constant.
So it's not possible to use the official TI TCAN4550 library with the official unmodified MSP430 library, without #undef-ing ID between them.
**Attention** This is a public forum