Part Number: MSP430FR6047
Hello,
I'm working on MSP430FR6047. I have a problem with the LFXT I connected a 32 kHz crystal oscillator with proper load caps. then loaded the example "msp430fr60x7_cs_05.c" and measured the frequency the output is around 37.5 kHz, not 32.768 kHz. I have changed the crystal and the caps. so I'm certain that the circuitry is good. plus I have tried different driver strength with no hope. I can see that OFIFG is always set and the code is traped in the do-while loop and the OFIFG can't be cleared.
I think this is the fail-safe clock which is 5MHz / 128.
so anyone has an idea.
Ahmed Mohsen
/* --COPYRIGHT--,BSD_EX
* Copyright (c) 2015, Texas Instruments Incorporated
* All rights reserved.
*
* Redistribution and use in source and binary forms, with or without
* modification, are permitted provided that the following conditions
* are met:
*
* * Redistributions of source code must retain the above copyright
* notice, this list of conditions and the following disclaimer.
*
* * Redistributions in binary form must reproduce the above copyright
* notice, this list of conditions and the following disclaimer in the
* documentation and/or other materials provided with the distribution.
*
* * Neither the name of Texas Instruments Incorporated nor the names of
* its contributors may be used to endorse or promote products derived
* from this software without specific prior written permission.
*
* THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
* AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
* THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
* PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
* CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
* EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
* PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
* OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
* WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
* OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
* EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
*
*******************************************************************************
*
* MSP430 CODE EXAMPLE DISCLAIMER
*
* MSP430 code examples are self-contained low-level programs that typically
* demonstrate a single peripheral function or device feature in a highly
* concise manner. For this the code may rely on the device's power-on default
* register values and settings such as the clock configuration and care must
* be taken when combining code from several examples to avoid potential side
* effects. Also see www.ti.com/grace for a GUI- and www.ti.com/msp430ware
* for an API functional library-approach to peripheral configuration.
*
* --/COPYRIGHT--*/
//******************************************************************************
// MSP430FR60xx Demo - Using LFXT in bypass mode, failsafe operation shown
//
// Description: ACLK is sourced from LFXT configured in bypass mode.
// An external 32768 Hz digital input signal is required for this example.
// When the signal is removed, ACLK defaults to LFMODOSC = 5MHz/128
// The LED blinks as long as the fault condition remains.
// Once the fault is fixed, LED goes OFF and ACLK is restored back to the
// digital input.
//
// ACLK = External digital in 32kHz, MCLK = SMCLK = 1MHz
//
// MSP430FR6047
// ---------------
// /|\| |
// | | |
// --|RST |
// | |
// | PJ.4/XIN |<-- External 32768Hz required!
// | P7.0 |--->ACLK
// | P1.0 |--->LED
//
// Cameron P LaFollette
// Texas Instruments Inc.
// November 2017
// Built with IAR Embedded Workbench V7.10 & Code Composer Studio V7.2
//******************************************************************************
#include <msp430.h>
int main(void)
{
WDTCTL = WDTPW | WDTHOLD;
// Configure GPIO
P1OUT = 0;
P1DIR |= BIT0; // LED setup
P7DIR |= BIT0;
P7SEL0 &= ~BIT0; // Output ACLK
P7SEL1 |= BIT0;
PJSEL0 |= BIT4;
// Disable the GPIO power-on default high-impedance mode to activate
// previously configured port settings
PM5CTL0 &= ~LOCKLPM5;
// XT1 Setup
CSCTL0_H = CSKEY_H; // Unlock CS registers
CSCTL1 = DCOFSEL_0; // Set DCO to 1MHz
CSCTL2 = SELA__LFXTCLK | SELS__DCOCLK | SELM__DCOCLK;
CSCTL3 = DIVA__1 | DIVS__1 | DIVM__1; // Set all dividers
CSCTL4 = LFXTBYPASS | HFXTOFF | LFXTOFF;
do
{
CSCTL5 &= ~LFXTOFFG; // Clear XT1 fault flag
SFRIFG1 &= ~OFIFG;
} while (SFRIFG1 & OFIFG); // Test oscillator fault flag
// Now that osc is running enable fault interrupt
SFRIE1 |= OFIE;
__bis_SR_register(LPM0_bits | GIE); // Wait in LPM0 for fault flag
__no_operation();
}
#if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__)
#pragma vector=UNMI_VECTOR
__interrupt void UNMI_ISR(void)
#elif defined(__GNUC__)
void __attribute__ ((interrupt(UNMI_VECTOR))) UNMI_ISR (void)
#else
#error Compiler not supported!
#endif
{
do
{
// set a breakpoint on the line below to observe XT1 operating from LFMODOSC
// when the breakpoint is hit during a crystal fault
CSCTL5 &= ~LFXTOFFG; // Clear XT1 fault flag
SFRIFG1 &= ~OFIFG;
P1OUT ^= BIT0;
__delay_cycles(25000); // time for flag to get set again
} while (SFRIFG1 & OFIFG); // Test oscillator fault flag
P1OUT &= ~BIT0;
}