This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Team MSP,
It seems that the FR5969 RTC_B can only be sourced from LFXTCLK (from an external xtal w/ LFXIN/LFXOUT). Usually MSP430 devices have a backup clock that auto-enables when a primary clock source fails.. for pretty much all peripherals.
Does the RTC_B peripheral have a backup clock source if the crystal(LFXIN/LFXOUT) -> LFXTCLK fails?
Thanks, Merril
Ref:
Hi Merril,
That sounds right. The TRM shows only the LFXTCLK as the clock source for RTC_B, and should that fail there is no mechanism to detect it and no other clock that is designated as a backup. Is this a customer question or issue?
Hi Dennis,
Thx! A customer ask.. looking for & wanting a backup if the XTAL fails..
Hi Merril,
You probably already saw this in the TRM. I forgot to add to the post.
Hi Dennis,
Thx! This seems to support the fact that there is no backup clock for RTC, right? Since the TRM says "If LFXT is sourcing any system clock (ACLK, MCLK, or SMCLK) and a fault is detected, the system clock is automatically switched to LFMODCLK for its clock source.".. so that provides backup for ACLK/MCLK/SMCLK.. but no backup clock for LFXT.. and then LFXT driving the RTC directly has no backup (for the RTC peripheral), right? This means that if LFXT fails.. the RTC will not function at all, right?
Thanks, Merril
**Attention** This is a public forum