Hi team,
What do I need to do with the Pin PJ.5/LFXOUT when using the LFXT bypass mode especially in an battery operated application to avoid leakage current?
Do I need an external pull-up / pull-down or can the pin be left floating?
As far as I understand it, the Pin PJ.5/LFXOUT is configured as an GPIO when using the bypass mode.
Therefore, following this comment from the TRM the pin PJ.5/LFXOUT should be left unconnected and then either be as an output or as an input with an pull-up / pull-down.
Is that correct or do I need an external pull-up / pull-down?
Thanks,
Marinus