Part Number: MSP430F413
Tool/software: Code Composer Studio
How you are calculating the 0xB7 , 0x12, etc.
const char digit[10] =
{
0xB7, /* "0" LCD segments a+b+c+d+e+f */
0x12, /* "1" */
0x8F, /* "2" */
0x1F, /* "3" */
0x3A, /* "4" */
0x3D, /* "5" */
0xBD, /* "6" */
0x13, /* "7" */
0xBF, /* "8" */
0x3F /* "9" */
};