Hi We have a product that has an 32768 Hz Crystal for RTC operations, and for communication purposes. The maximum allowable BaudRate using the crystal is 9600 bps, and we would like to extend this baudrate to the double. Is the MSP430 capable of working with a 65535 Hz Crystal maintaining the stability and being able to use the rtd and the uart ? Do you see any drawback in doing this ? I 've been looking for this data within the datasheet and I could find it. Thanks in advance.