This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: Code Composer Studio
how can i use onboard button P2.6 on the launchpad
A code example which showcases the functionality that Mike explains above is provided in the TI Resource Explorer ( msp430fr413x_P1_01.c ).
The only change you would have to make in the code is to set the input to be Port 2 Pin 6 and not Port 1 Pin 3.
Best regards,
Matt
**Attention** This is a public forum