Part Number: MSP432P401R
Other Parts Discussed in Thread: ENERGIA
hi, i trying to write a code that set the output voltage to a fix level. and i want to keep it at that level, whatever happens. So when the i connects a heavy load, this shouldn't affect the output. I know To get that working, you need to change the input signals to the circuit. I know that arduino have a library called PID library that does that, what that library does is to crate a stable control of the output, by measuring the difference with the desired output (error), using other factors (such as history) and changing the input signal (feedback) until balance is achieved ad the difference between the desired output and the actual current value is called the error. P stands for proportional, I for Integral, D for differential. These are the mathematical terms that play a role in the calculations inside the PID library, is there any library that act like that or is there any PID library for MSP 432 that i can use
thank you.
When you build a power supply, you want to set the output voltage to a fixed level. And you want to keep it at that level, whatever happens.
When the user connects a heavy load, this shouldn't affect the output.
To get that working, you need to change the input signals to the circuit.
But how do you do that? How much change? How fast? How to prevent that the change pushes the output above the level?
And what if the load is removed?
That's a problem that the PID mechanism tries to resolve:
a stable control of the output, by measuring the difference with the desired output (error), using other factors (such as history) and changing the input signal (feedback) until balance is achieved.
The difference between the desired output and the actual current value is called the error.
P stands for proportional, I for Integral, D for differential. These are the mathematical terms that play a role in the calculations inside the PID library