Need help. Did I forget something when I unzipped the slaa290 file?
I've included the RTC.h file in my main.c project file as well as copying the RTC.h file to the TI CCS MSP430 include directory, but I get the following errors
> #include "msp430g2231.h"
> #include "RTC.h"
unresolved symbol TI_second, first referenced in ./main.obj
unresolved symbol TI_PM, first referenced in ./main.obj
unresolved symbol TI_minute, first referenced in ./main.obj
unresolved symbol TI_hour, first referenced in ./main.obj
Console Output:
'Invoking: Linker'
"C:/Program Files/Texas Instruments/ccsv4/tools/compiler/MSP430 Code Generation Tools 3.3.2/bin/cl430" -vmsp -g --define=__MSP430F2001__ --define=__MSP430G2231__ --diag_warning=225 --printf_support=minimal -z -m"PositionSensor.map" --stack_size=50 --heap_size=0 --warn_sections -i"C:/Program Files/Texas Instruments/ccsv4/msp430/include" -i"C:/Program Files/Texas Instruments/ccsv4/tools/compiler/MSP430 Code Generation Tools 3.3.2/lib" -i"C:/Program Files/Texas Instruments/ccsv4/tools/compiler/MSP430 Code Generation Tools 3.3.2/include" --reread_libs --rom_model -o "PositionSensor.out" "./main.obj" -l"libc.a" "C:/Program Files/Texas Instruments/ccsv4/msp430/include/lnk_msp430g2231.cmd"
<Linking>
undefined first referenced
symbol in file
--------- ----------------
TI_PM ./main.obj
TI_hour ./main.obj
TI_minute ./main.obj
TI_second ./main.obj
error: unresolved symbols remain
error: errors encountered during linking; "PositionSensor.out" not built