Other Parts Discussed in Thread: MSP430F5438A
Tool/software: Code Composer Studio
Hello I am very new to the msp430 microcontrollers. now iam finding difficult to run usci uartA1 backchannel to echo characters using msp430 driverlib. Here is my code taken from example codes with slight changes made for using uart backchannel. Hope i could get the problem solved. I think i have done everything correctly, please let me know where i went wrong.
/* --COPYRIGHT--,BSD
* Copyright (c) 2017, Texas Instruments Incorporated
* All rights reserved.
*
* Redistribution and use in source and binary forms, with or without
* modification, are permitted provided that the following conditions
* are met:
*
* * Redistributions of source code must retain the above copyright
* notice, this list of conditions and the following disclaimer.
*
* * Redistributions in binary form must reproduce the above copyright
* notice, this list of conditions and the following disclaimer in the
* documentation and/or other materials provided with the distribution.
*
* * Neither the name of Texas Instruments Incorporated nor the names of
* its contributors may be used to endorse or promote products derived
* from this software without specific prior written permission.
*
* THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
* AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
* THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
* PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
* CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
* EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
* PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
* OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
* WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
* OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
* EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
* --/COPYRIGHT--*/
//******************************************************************************
//! This example shows how to configure the UART module as the loopback to
//! verify that received data is sent data.
//!
//! MSP430F5438A
//! -----------------
//! RST -| P3.4/UCA0TXD|----|
//! | | |
//! | | |
//! | P3.5/UCA0RXD|----|
//! | |
//!
//!
//! This example uses the following peripherals and I/O signals. You must
//! review these and change as needed for your own board:
//! - UART peripheral
//! - GPIO Port peripheral (for UART pins)
//! - UCA0TXD
//! - UCA0RXD
//!
//! This example uses the following interrupt handlers. To use this example
//! in your own application you must add these interrupt handlers to your
//! vector table.
//! - USCI_A0_VECTOR.
//******************************************************************************
#include "driverlib.h"
//*****************************************************************************
//
//Select Baud rate
//
//*****************************************************************************
#define BAUD_RATE 9600
//*****************************************************************************
//
//Initialize received data
//
//*****************************************************************************
uint8_t receivedData = 0x00;
//*****************************************************************************
//
//Initialize trasnmit data
//
//*****************************************************************************
uint8_t transmitData = 0x00;
uint8_t check = 0;
void main (void)
{
//Stop WDT
WDT_A_hold(WDT_A_BASE);
//P3.4,5 = USCI_A0 TXD/RXD
GPIO_setAsPeripheralModuleFunctionInputPin(
GPIO_PORT_P4,
GPIO_PIN4 + GPIO_PIN5
);
//Baudrate = 9600, clock freq = 1.048MHz
//UCBRx = 109, UCBRFx = 0, UCBRSx = 2, UCOS16 = 0
USCI_A_UART_initParam param = {0};
param.selectClockSource = USCI_A_UART_CLOCKSOURCE_SMCLK;
param.clockPrescalar = 109;
param.firstModReg = 0;
param.secondModReg = 2;
param.parity = USCI_A_UART_NO_PARITY;
param.msborLsbFirst = USCI_A_UART_LSB_FIRST;
param.numberofStopBits = USCI_A_UART_ONE_STOP_BIT;
param.uartMode = USCI_A_UART_MODE;
param.overSampling = USCI_A_UART_LOW_FREQUENCY_BAUDRATE_GENERATION;
if (STATUS_FAIL == USCI_A_UART_init(USCI_A1_BASE, ¶m)){
return;
}
//Enable UART module for operation
USCI_A_UART_enable(USCI_A1_BASE);
//Enable Receive Interrupt
USCI_A_UART_clearInterrupt(USCI_A1_BASE,
USCI_A_UART_RECEIVE_INTERRUPT);
USCI_A_UART_enableInterrupt(USCI_A1_BASE,
USCI_A_UART_RECEIVE_INTERRUPT);
__enable_interrupt();
while (1)
{
transmitData = transmitData+1; // Increment TX data
// Load data onto buffer
USCI_A_UART_transmitData(USCI_A1_BASE,
transmitData);
while(check != 1);
check = 0;
}
}
//******************************************************************************
//
//This is the USCI_A0 interrupt vector service routine.
//
//******************************************************************************
#if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__)
#pragma vector=USCI_A1_BASE
__interrupt
#elif defined(__GNUC__)
__attribute__((interrupt(USCI_A1_BASE)))
#endif
void USCI_A1_ISR (void)
{
switch (__even_in_range(UCA1IV,4)){
//Vector 2 - RXIFG
case 2:
receivedData = USCI_A_UART_receiveData(USCI_A1_BASE);
if(!(receivedData == transmitData)) // Check value
{
while(1);
}
check =1;
break;
default: break;
}
}