Hey all,
Is it possible to use the uC without this crystal stably? I mean without resetting itself from time to time.
Is it possible to use PWM and UART simultaneously since they use TIMER_A?
thank u
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hey all,
Is it possible to use the uC without this crystal stably? I mean without resetting itself from time to time.
Is it possible to use PWM and UART simultaneously since they use TIMER_A?
thank u
Hi Hasith,
Hasith Ishara Kulathilaka said:I mean without resetting itself from time to time.
Did you disable the Watchdog Timer? i.e.
// disable watchdog timer
//------------------------
WDTCTL = WDTPW + WDTHOLD; // Stop WDT
Should be the first instruction of your application! If you will use it in your application you can re-enable it later!
Hasith Ishara Kulathilaka said:Is it possible to use PWM and UART simultaneously since they use TIMER_A?
No, you need to stop the PWM for doing the UART communication and vice versa. If you need both simultaneously, you should use a device with a hardware UART or at least two timers.
Rgds
aBUGSworstnightmare
**Attention** This is a public forum