This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: Code Composer Studio
Hi,
I was trying to flash the MSP430FW427 but an error throw by CCS "The Debug Interface to the device has been secured". I had gone through some post's but those options are not visible on CCS lastest version. Kindly help me in this regard.
Hi Vijay,
How many devices show this issue, just one?
Which board / programming tool are you using for programming the device?
Have you used this device already for programming successfully?
Best regards
Lukas
Hi Lukas,
How many devices show this issue, just one?
Yes, Just one. (I had tried on only one IC, just I'm getting started on MSP430FW427)
Which board/programming tool are you using for programming the device?
MSP-FET Flash emulation tool
Have you used this device already for programming successfully?
No, Since from the first time I try to flash it throws an error.
Hi Vijay,
Thanks for your reply.
Do you have maybe a further FW427 device for cross check?
Lukas
Hi Lukas,
Thanks for the reply.
No, I have not cross-checked with further FW427 because it was soldered on PCB. Do you mean it is the problem with FW427? Do I need to replace it with a new one?
Hi Vijay,
I would at least do a cross check if the tools have an issue or really the device.
Lukas
Hi Lukas,
Thanks for the reply.
I had crossed checked the connections and flash emulation tool was new one bought from TI Store.
FW427 - Flashing Tool (Pin Connections)
Pin 54 - Pin 1
Pin 55 - Pin 3
Pin 56 - Pin 5
Pin 57 - Pin 7
Pin 58 - Pin 11
Hi Vijay,
Is the issue still present?
If yes, you can order some more samples of FW427 and check with the new devices if it works.
Best regards
Lukas
**Attention** This is a public forum