This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: MSP-EXP430G2
Hi.
I'm graduating Telecomunications engeneering in a brazilian institution, came through this forum ask about the power supply of the msp430, it needs 3.6V to power up? When it power up how fast i can transfer a information to another device?
all the best,
Willian.
Hi,
For G2 device, it can run under 1.8V to 3.6V. If you want to keep it run under 16MHz, you need to supply at least 3.3V.
About "When it power up how fast i can transfer a information to another device?", one is hardware setup time another is software setup time.
For hardware setup time, you can refer to this:
Eason
**Attention** This is a public forum