This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: BOOSTXL-SENSORS
Hello,
I'm configuring Boostxl-sensors with TM4C123G through I2C protocol, BMI160 and OPT3001 worked successfully, but i have two problems with BME280 and BMM150.
First, when i configured BME280, it didn't work and when i tried to debug the code, I've noticed that when i write any value at any register and then trying to read the same register always the read value is the default value of the register,that means that i can't write any value to the sensor registers. note that the I2C driver that i used is tested before and it works.
does that mean that the sensor is broken ?
Second , i configured BMM150 (the auxiliary sensor ) by BMI160 through the secondary I2C, but the output values are not even close the predicted values.
So , Is there any examples to help me to find out my problem ?
Hi,
As I check, BMM150 belong to bosch.
Have you check the website:http://www.ti.com/tool/BOOSTXL-SENSORS?keyMatch=BOOSTXL-SENSORS&tisearch=Search-EN-everything&usecase=part-number
I found it has software example.
Eason
**Attention** This is a public forum