This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP432P401R: Queries SPI driver API's with TI RTOS example in SDK

Part Number: MSP432P401R

Hello All,

I am new to TI MCU's and the code base.

I have found good amount of example for all the peripherals in the SDK. I have one very basic query, not in particular to SPI but I need any reference to address my query so I will SPI as an example.

In the SDK examples for SPI with TI RTOS, I have observed few API's like below. where it's not clear how the Port& Pins are configured, which channel the SPI is configured for and other information.

SPI_Params_init

SPI_open

SPI_transfer

Because in example with no-rtos, it's clear that first pin configuration and then enabling the master with channel address like EUSCI_B0_BASE.

Can someone help me to understand this. I have gone through the TI-rtos document but that didn't help.

**Attention** This is a public forum