This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430FR2476: ADC Veref+ and Veref- and Channel input

Part Number: MSP430FR2476
Other Parts Discussed in Thread: MSP-FET

I am planning to use the Veref+ and Veref- ADC inputs In the data sheet, I cannot find a specification on the range of acceptable values of external ADC Channels or Verefs. 

Is Veref+ capable of a value of DVCC? What if using the internal ADC Buffer?

Is Veref- capable of a value of DVSS?

If Veref- is set to a value between DVCC and DVSS, and the Channel Input is below the Veref-, can damage occur? Will the ADC result be zero or something unknown?

What is the input range spec for Channel inputs?

The multiplexed pin for Veref+ is also A0 and Veref- is also A2, according to the Datasheet (though there is discrepancy in Table 4-2, Signal Descriptions). When programming a sequence of conversions, the ADC always decrements to A0. If using Veref+ and Veref-, what will be the expected results of A0 and A2 conversions?

**Attention** This is a public forum