Hi,
i need to validate the ICS43434(Acoustic sensor) which is connected to MSP432P411VIPZ using I2S interface.
As we know that I2S interface is not available on MSP432P411VIPZ, i need to mimic the SPI to act as I2S interface.
if there is any reference code that can be used to mimic the SPI as I2S, will be very helpful.
with regards to the below given link:
https://e2e.ti.com/support/microcontrollers/msp430/f/166/t/547391?MSP432-I2S-implementation
what is the input given here?
whether this code can be used for mimic the SPI as I2S interface?, if yes, whether the project code is available to be shared?
Thank you,
Maniram