Part Number: MSP430I2021
Hi experts,
My customer has a question about the RST pin.
Could you tell me about the following items?
1)Is it okay to connect the RST pin directly to the VDD level?
2)If the RST pin is directly connected to the VDD level, will CPU reset work properly when an interrupt for a non-maskable reset request such as WDT interrupt is received?
3)Is there an internal circuit for the RST pin of the MSP 430I2021?
I checked it in the thread below, but I couldn't get an answer, so I will check it again.
https://e2e.ti.com/support/microcontrollers/msp430/f/166/p/903189/3338653#3338653
Best Regards,
O.H