This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi..
I'm using a MSP-FET430UIF debug interface and MSP430FG437 device.In the CCSV4 IDE if I run the blink led code I get the following error:
"Error initializing emulator:
A firmware update is required for the USB debug interface.
Click the "Update" button to update the firmware and launch your debug session."
How do I resolve the problem without updating the firmware. Also i have one more question, if the firmware is updated will the debugger still work with CCE or CCS version below CCSV4?
Using the MSP-FET430UIF I have always let the system update the firmware, and as of yet I haven't had any problems. I even one time lost power right in the middle of a flash update, and the next time I tried to use the MSP-FET430UIF, I was promted to update the firmware and it worked. Do not update the firmware of the EZ430, as this will make it stop working.
**Attention** This is a public forum