This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: TI C/C++ Compiler
Hi,
I am trying to generate an Elf file with constant data located in the INFOD MEMORY area. I am using the MSP-CGT 18.12.4.LTS compiler suite and the standard linker command file for the MSP430F2132 microcontroller provided by CCS v9.3 which defines the INFOD MEMORY area as follows:
INFOD : origin = 0x1000, length = 0x0040
and the section directive:
.infoD : {} > INFOD
My source file contains the following instructions:
#pragma DATA_SECTION(C_initialCalibPrm,".infoD"); const t_NvmData C_initialCalibPrm = 0x0000;
At link time I get the following error message: warning: section executable.elf(.infoD) at 01000h falls in unconfigured memory (skipped), while the MEMORY area seems properly configured in the linker command file for me.
Any idea on the origin of this problem?
Thanks in advance.
I tried the two proposed solutions without success:
.infoD 0 00001000 00000010 UNINITIALIZED
So, the generated Elf files does not permit to program that area.
Hi Jerome,
You might try replacing
#pragma DATA_SECTION
with
#pragma CODE_SECTION
to program the flash. You can find more info in Section 5.11.5 in the compiler UG.
https://www.ti.com/lit/ug/spnu151v/spnu151v.pdf?ts=1594922986245
BR,
Leo
Hi Leo,
I tried your proposition. At compilation time I get the following warning message:
warning: pragma CODE_SECTION can only be applied to a function definition, not "C_initialCalibPrm"
In the generated Elf and map files, the infoD section is kept empty:
MEMORY CONFIGURATION name origin length used unused attr fill ---------------------- -------- --------- -------- -------- ---- -------- INFOD 00001000 00000040 00000000 00000040 RWIX
So this solution does not seem to solve the problem
**Attention** This is a public forum