This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/MSP430FR5964: MSP430FR5964 Header file wrong in CCS 10.10

Part Number: MSP430FR5964

Tool/software: Code Composer Studio

Hi,

I´ve discovered that the header file for the MSP430FR5964 is missing port definitions starting with line 3582. I`ve attached the working header from CCS10.00 and the non-working from CCS 10.10. If you dif those two you will see that there is no definition for baseaddresses port 2,3, etc. If you use this header in conjunction with the driverlib the output register won´t be set!

Best regards

Steffen

msp430fr5964_CCS1010.h

msp430fr5964_CCS1000.h

  • Hi Steffen,

    Thank you for your feedback. I will do the test. If the 10.10 version header does have the problem you described, I will report to the CCS Team for modification.
    Thanks again!

    Best Regards

    Johnson

**Attention** This is a public forum