This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I am using MSP430FR5994 with MSP-GCC (Not using CCS)
I want to store some parameters in the FRAM which will be updated in each cycle and the values will be changed on the FRAM
I created my variables using persistent as follows
__attribute__ ((persistent)) uint8_t fNum_T = 1;
And in the main I disable the MPU and increment the persistent variable
MPUCTL0 = MPUPW | MPUENA_0; // Write PWD to access MPU registers and disable the MPU
fNum_T++;
I expect that this variable should increase by 1 every time I turn off and on the power but I observe that the value stays the same i.e. 1.
The persistent variable is created as when I program I see 2 bytes assigned to section .persistent
However I cannot modify the variable. Do I need to change something else in the MPU? What step am I missing?
Hi Cash,
Thank you for the reference. I was able to solve the issue.
Best,
Dhanashree Vaidya
**Attention** This is a public forum