This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I would like to know about some question about PMM29 errata on MSP430fR6877.
I am considering implementing workaround 3 for PMM29.
And I would like to use watch dog timer.
But according the Note, it is described that if the WDT triggers PUC reset during LPM2/3/4, workaround 3 doesn't make sense and lockup will occur.
Could you confirm about following question?
1.I understood that I should only pay attention to WDT triggers because all other PUC triggering factors do not occur during LPM. Is my understanding correct?
2.If I followed Note about workaround 3 and the program hangs during an interrupt other than the WDT interval timer interrupt, I think that it cannot be reset by the WDT interval timer interrupt unless nested interrupt are enabled.
Is my understanding correct?
If yes, Is there a way not to enable nested interrupt but reset the hang of the program during interrupt processing in workaround3 case?
Regards,
U-SK
Hello U-SK,
Thanks for your patientence.
1. Correct. According to the note, only the WDT timeout PUC during LPM mode is the concern.
2. I think your understanding here is also correct. Without nested interrupts, I don't see how the WDT interval mode can protect against a hang in an ISR.
Again, I don't see a great way to protect those sections of code with the WDT, but maybe you can poll the WDTIFG flag inside all loops in the ISRs as a possible breakout?
That's my only idea currently.
Thanks,
JD
Hi JD,
Thank you for your reply.
I think your advice is a safe way to prevent hangs during interrupt processing!
But with your advice, I am worried that it may not be possible to deal with malfunctions of the microcomputer due to noise.
How about the idea below?
Are there any concerns when compared to the watch dog mode of WDT?
-In TimerA0, set Continuous mode and Output mode 5 (Reset).
-Connect TA0.1 and RST pin externally
-Update by incrementing the interval value you want to set periodically to CCR1.
We are considering whether the above is worth a try...
Regards,
U-SK
Hi TI team,
I found that this solution may cause an unintentional reset because the program cannot know the exact counter value.
So I am considering following method.
-In TimerA0, set Continuous mode and Output mode 5 (Reset).
-Connect TA0.1 and RST pin externally
-The program periodically sets the TAxR register to 0 before the counter reaches CCR1.
I think this method requires one timer module for WDT but it should works well.
What do you think of this method as a countermeasure for PMM29?
Are there any concerns?
Regards,
U-SK
Hello U-SK,
For the WDT timer idea, what is the concern about noise? Alternatively, I guess you could technically configure the WDT for normal operation at beginning of an ISR, and then switch it back to interval mode at the end, but this will add additional processing time to all interrupts.
Your idea is quite interesting. I think it would protect against the code hanging in an ISR, but my concern is mainly on how to connect the MSP430 to try and drive its own /RST line as Its definitely not standard. It would generate a BOR reset, which means the MSP430 will come back up with the GPIOs configured as inputs, but it's not clear exactly when this happens while entering reset.
RST pin minimum timing requirement is below. I guess we can't be sure about the timing, but we can probably make the assumption that the GPIO will stay low until the MSP430 resets and releases it...
Also, since the reset is from the external reset, there will be no way for the software to tell the difference between an actual external reset or the timeout reset, but I don't think that knowing this is that important to the application.
Finally, adding another connection to RST could possibly add extra noise/capacitance. I think it should be a short trace, in this case, but still something to be slightly cautious of.
Overall, I believe your solution will work, but I have not seen it done before so you probably test it. Do you have any MSP430 launchpads?
Thanks,
JD
Hi JD,
Thank you for your advice.
>For the WDT timer idea, what is the concern about noise?
Yes.
>Alternatively, I guess you could technically configure the WDT for normal operation at beginning of an ISR, and then switch it back to interval mode at the end, but this will add additional processing time to all interrupts.
Thank you for your advice. I will confirm with my customer about your solution.
I confirmed about your concern using PWM example project with MSP430FR5969 Launchpad.
But following problems is appeared.
・When the PxSEL register is set as the Timer pin, the pin goes low even if pullup.
Therefore, BOR reset occurs at the moment in case PWM pin and RST pin is connected together.
・OUTMOD_5 does not change the signal when it starts from Low output.
I think it is necessary to prevent the signal from going low at all until the PWM goes high.
Are there any good solution?
Regards,
U-SK
Hi JD,
I'll inform you of some update information.
I took the following measures.
・Use the NMI function instead of the RST function so that NMI occurs on the rising edge.
・Output PWM signal set as continuous mode, output mode 7.
As a result, NMI occurred at the intended timing, and the reset due to WDT Password violation worked fine.
It also works well even during peripheral interrupts.
The only concern I found was that JTAG did not work and I could not debug or programming while connecting the PWM port to the NMI pin.
Is there any way to deal with this other than disconnecting the signal when debugging and programming?
Do you find any other concerns in my overall countermeasure?
>Alternatively, I guess you could technically configure the WDT for normal operation at beginning of an ISR, and then switch it back to interval mode at the end, but this will add additional processing time to all interrupts.
->I confirmed to my customer about your advise.
My customer is concerned about the increase in processing time of the entire application due to the mode switching of WDT each time.
Best Regards,
U-SK
Happy New Year,
Sorry for the delay. Were you able to work around the issue with the timer output going low? I was going to run a timer example on a launchpad, but didn't have a chance to do it before the Holidays.
As for the interference with JTAG, can you share your connections between the PWM port and the RST/NMI pin? I'm guessing that the PWM pin is connected directly, so when it's driving the pin high, the JTAG can not take control of it. Most likely, the PWM signal is high, but JTAG is trying to pull RST low. Is this correct?
You would definitely want to try to find a configuration that still enables JTAG. You would want some sort of open-drain configuration, that would allow JTAG RST to still drive the pin low. I think that maybe if you put a series resistor between RST/NMI and the PWM pin, that could work. Something small enough compared to the pull-up that should be on the RST line, maybe like 1-5k ohm. You could also implement some sort of external pull-down only circuit.
Does that make sense?
JTAG can be sensitive to signal timing which can be affected by the resistance and capacitance on the line. Since we are coming up with this external workaround right now, it is possible that this configuration interferes slightly with that timing. I think the impact will be minimal, but you will need to test it once the circuit is setup.
Thanks,
JD
**Attention** This is a public forum