Tool/software: Code Composer Studio
Hello
I wrote firmware for a certain project of mine using the Launchpad of msp430fr2433. Now I want to design a custom board that just has the micro and can be programmed using the launchpad.
I designed the board and made manual connections with the required pins and connected them to the J101 on the launchpad. I connected SDWTCK, SBWTDIO, P1.4, P1.5, 5V, and Gnd. I also pulled SBWTDIO high with a 47K resistor.
Could you please review my schematic and let me know if it's good? I want to double-check before I order this board.